我们使用的是MIMXRT1052CVJ5B的芯片,请问现在需要设计前的功耗估算,外设使用的情况:2个串口通信,外挂4个从设备的LPI2C2,PWM1输出,2个GPIO输入,驱动分辨率为800*480的LCD屏(RGB565),外挂1个从设备的LPI2C1,外挂时钟频率为133MHz的SPI nor flash,外挂带宽为166MHz的SDRAM。
请问这里各个电源轨(vdd_soc_in,vdd_high_in,vdd_snvs_in,vdd_adc...)的功耗如何估计,谢谢!
i.MX-RT1050