RT1020 bootloader flash linked code sample (IAR)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1020 bootloader flash linked code sample (IAR)

2,486 Views
JamesNgo
Contributor III

I need a second flash linked/XIP bootloader in my design to manage selecting which fw application (programmed also on QSPI flash different regions) -- a typical and popular design discussed here.

I couldn't find the flash linked bootloader code for rt1020 repo. However I dug in the forums to find it is included in AN12604SW.zip?!. Questions:

AN12604SW bootloader appears to have maybe 20% of the ram resident flashloader in terms of functionality/blhost commands and works only with DEBUG turned on... Do you have a fully compatible flash linked bootloader wrt flashloader? Or way to configure RAMloader to flash linked bootloader?

Thanks

Labels (1)
0 Kudos
Reply
2 Replies

2,470 Views
jeremyzhou
NXP Employee
NXP Employee

Hi @JamesNgo ,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Actually, the AN12304SW provides the second bootloader based on XIP, which definitely meets your requirement.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

2,480 Views
mjbcswitzerland
Specialist V
0 Kudos
Reply