RT1011 Flashloader

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RT1011 Flashloader

1,953 次查看
nxf58843
NXP Employee
NXP Employee

When using the flashloader as described in AN12238 with RT1011, replace the commands on pages 11 and 12 with these:

>sdphost.exe -u 0x1fc9,0x0145 -- error-status

>sdphost.exe -u 0x1fc9,0x0145 -- write-file 0x20205800 "..\..\Mfgtools-rel\Profiles\MXRT101X\OS Firmware\ivt_flashloader.bin"

>sdphost.exe -u 0x1fc9,0x0145 --jump-address 0x20205800

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,947 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hello  nxf58843

   Dear colleague, do you want to share the experience, or have any question about the rt1010 flashloader?

   In fact, about the sdphost related commander for RT1010, I highly recommend you use the MCUBootutility, that will list all the related log.

https://github.com/JayHeng/NXP-MCUBootUtility/archive/v2.4.0.zip
the related user manual is:
https://github.com/JayHeng/NXP-MCUBootUtility

 

Wish it helps you!

If you still have questions about it, please kindly let me know!

Best Regards,

Kerry

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

-----------------------------------------------------------------------------

0 项奖励
回复