RT Linux Compile errors

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT Linux Compile errors

7,073 Views
os
Contributor I

I am trying to build the imx realtime linux kernel for machine: imx6qsabresd.

bitbake -c compile linux-fslc-imx-rt. Getting compile errors related to gpu-viv. Please help!

LD      drivers/net/ethernet/cirrus/built-in.o

|   CC      drivers/input/keyboard/snvs_pwrkey.o

| In file included from /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/include/linux/seqlock.h:35:0,

|                  from /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/include/linux/time.h:5,

|                  from /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/include/linux/stat.h:18,

|                  from /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/include/linux/module.h:10,

|                  from /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/drivers/mxc/gpu-viv/hal/os/linux/kernel/gc_hal_kernel_linux.h:61,

|                  from /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/drivers/mxc/gpu-viv/hal/os/linux/kernel/gc_hal_kernel_os.c:56:

| /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/drivers/mxc/gpu-viv/hal/os/linux/kernel/gc_hal_kernel_os.c: In function 'gckOS_WaitSignal':

| /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/drivers/mxc/gpu-viv/hal/os/linux/kernel/gc_hal_kernel_os.c:7365:23: error: passing argument 1 of '_raw_spin_lock_irq' from incompatible pointer type [-Werror=incompatible-pointer-types]

|      raw_spin_lock_irq(&signal->obj.wait.lock);

|                        ^

| /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/include/linux/spinlock.h:239:53: note: in definition of macro 'raw_spin_lock_irq'

|  #define raw_spin_lock_irq(lock)  _raw_spin_lock_irq(lock)

|                                                      ^

| In file included from /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/include/linux/spinlock.h:281:0,

|                  from /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/include/linux/seqlock.h:35,

|                  from /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/include/linux/time.h:5,

|                  from /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/include/linux/stat.h:18,

|                  from /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/include/linux/module.h:10,

|                  from /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/drivers/mxc/gpu-viv/hal/os/linux/kernel/gc_hal_kernel_linux.h:61,

|                  from /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/drivers/mxc/gpu-viv/hal/os/linux/kernel/gc_hal_kernel_os.c:56:

| /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/include/linux/spinlock_api_smp.h:29:17: note: expected 'raw_spinlock_t * {aka struct raw_spinlock *}' but argument is of type 'spinlock_t * {aka struct spinlock *}'

|  void __lockfunc _raw_spin_lock_irq(raw_spinlock_t *lock)

|                  ^

| /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/drivers/mxc/gpu-viv/hal/os/linux/kernel/gc_hal_kernel_os.c:7387:9: error: implicit declaration of function 'DEFINE_SWAITER' [-Werror=implicit-function-declaration]

|          DEFINE_SWAITER(wait);

|          ^

| /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/drivers/mxc/gpu-viv/hal/os/linux/kernel/gc_hal_kernel_os.c:7387:24: error: 'wait' undeclared (first use in this function)

|          DEFINE_SWAITER(wait);

|                         ^

| /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/drivers/mxc/gpu-viv/hal/os/linux/kernel/gc_hal_kernel_os.c:7387:24: note: each undeclared identifier is reported only once for each function it appears in

| /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/drivers/mxc/gpu-viv/hal/os/linux/kernel/gc_hal_kernel_os.c:7388:9: error: implicit declaration of function 'swait_prepare_locked' [-Werror=implicit-function-declaration]

|          swait_prepare_locked(&signal->obj.wait, &wait);

|          ^

| In file included from /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/include/linux/spinlock.h:281:0,

|                  from /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/include/linux/seqlock.h:35,

|                  from /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/include/linux/time.h:5,

|                  from /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/include/linux/stat.h:18,

|                  from /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/include/linux/module.h:10,

|                  from /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/drivers/mxc/gpu-viv/hal/os/linux/kernel/gc_hal_kernel_linux.h:61,

|                  from /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/drivers/mxc/gpu-viv/hal/os/linux/kernel/gc_hal_kernel_os.c:56:

| /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/drivers/mxc/gpu-viv/hal/os/linux/kernel/gc_hal_kernel_os.c:7400:33: error: passing argument 1 of '__raw_spin_unlock_irq' from incompatible pointer type [-Werror=incompatible-pointer-types]

|              raw_spin_unlock_irq(&signal->obj.wait.lock);

|                                  ^

| /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/include/linux/spinlock_api_smp.h:79:58: note: in definition of macro '_raw_spin_unlock_irq'

|  #define _raw_spin_unlock_irq(lock) __raw_spin_unlock_irq(lock)

|                                                           ^

| /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/drivers/mxc/gpu-viv/hal/os/linux/kernel/gc_hal_kernel_os.c:7400:13: note: in expansion of macro 'raw_spin_unlock_irq'

|              raw_spin_unlock_irq(&signal->obj.wait.lock);

|              ^

| /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/include/linux/spinlock_api_smp.h:164:20: note: expected 'raw_spinlock_t * {aka struct raw_spinlock *}' but argument is of type 'spinlock_t * {aka struct spinlock *}'

|  static inline void __raw_spin_unlock_irq(raw_spinlock_t *lock)

|                     ^

| In file included from /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/include/linux/seqlock.h:35:0,

|                  from /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/include/linux/time.h:5,

|                  from /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/include/linux/stat.h:18,

|                  from /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/include/linux/module.h:10,

|                  from /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/drivers/mxc/gpu-viv/hal/os/linux/kernel/gc_hal_kernel_linux.h:61,

|                  from /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/drivers/mxc/gpu-viv/hal/os/linux/kernel/gc_hal_kernel_os.c:56:

| /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/drivers/mxc/gpu-viv/hal/os/linux/kernel/gc_hal_kernel_os.c:7402:31: error: passing argument 1 of '_raw_spin_lock_irq' from incompatible pointer type [-Werror=incompatible-pointer-types]

|              raw_spin_lock_irq(&signal->obj.wait.lock);

|                                ^

| /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/include/linux/spinlock.h:239:53: note: in definition of macro 'raw_spin_lock_irq'

|  #define raw_spin_lock_irq(lock)  _raw_spin_lock_irq(lock)

|                                                      ^

| In file included from /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/include/linux/spinlock.h:281:0,

|                  from /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/include/linux/seqlock.h:35,

|                  from /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/include/linux/time.h:5,

|                  from /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/include/linux/stat.h:18,

|                  from /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/include/linux/module.h:10,

|                  from /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/drivers/mxc/gpu-viv/hal/os/linux/kernel/gc_hal_kernel_linux.h:61,

|                  from /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/drivers/mxc/gpu-viv/hal/os/linux/kernel/gc_hal_kernel_os.c:56:

| /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/include/linux/spinlock_api_smp.h:29:17: note: expected 'raw_spinlock_t * {aka struct raw_spinlock *}' but argument is of type 'spinlock_t * {aka struct spinlock *}'

|  void __lockfunc _raw_spin_lock_irq(raw_spinlock_t *lock)

|                  ^

| /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/drivers/mxc/gpu-viv/hal/os/linux/kernel/gc_hal_kernel_os.c:7423:9: error: implicit declaration of function 'swait_finish_locked' [-Werror=implicit-function-declaration]

|          swait_finish_locked(&signal->obj.wait, &wait);

|          ^

| In file included from /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/include/linux/spinlock.h:281:0,

|                  from /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/include/linux/seqlock.h:35,

|                  from /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/include/linux/time.h:5,

|                  from /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/include/linux/stat.h:18,

|                  from /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/include/linux/module.h:10,

|                  from /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/drivers/mxc/gpu-viv/hal/os/linux/kernel/gc_hal_kernel_linux.h:61,

|                  from /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/drivers/mxc/gpu-viv/hal/os/linux/kernel/gc_hal_kernel_os.c:56:

| /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/drivers/mxc/gpu-viv/hal/os/linux/kernel/gc_hal_kernel_os.c:7426:25: error: passing argument 1 of '__raw_spin_unlock_irq' from incompatible pointer type [-Werror=incompatible-pointer-types]

|      raw_spin_unlock_irq(&signal->obj.wait.lock);

|                          ^

| /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/include/linux/spinlock_api_smp.h:79:58: note: in definition of macro '_raw_spin_unlock_irq'

|  #define _raw_spin_unlock_irq(lock) __raw_spin_unlock_irq(lock)

|                                                           ^

| /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/drivers/mxc/gpu-viv/hal/os/linux/kernel/gc_hal_kernel_os.c:7426:5: note: in expansion of macro 'raw_spin_unlock_irq'

|      raw_spin_unlock_irq(&signal->obj.wait.lock);

|      ^

| /home/oswald/workspace/poky_jethro/build-imx6/tmp/work-shared/imx6qsabresd/kernel-source/include/linux/spinlock_api_smp.h:164:20: note: expected 'raw_spinlock_t * {aka struct raw_spinlock *}' but argument is of type 'spinlock_t * {aka struct spinlock *}'

|  static inline void __raw_spin_unlock_irq(raw_spinlock_t *lock)

|                     ^

Labels (1)
0 Kudos
Reply
1 Reply

6,526 Views
igorpadykov
NXP Employee
NXP Employee

Hi Oswald

official nxp bsp provides linux images as described in

attached Table 1. Freescale Yocto project images.

rt linux is provided by community, so one can post that on

meta-fsl-arm mailing list, so that someone familiar with it could try to assist you.

https://lists.yoctoproject.org/listinfo/meta-freescale

Differencies between nxp and community releases are described in

FSL Community BSP Release Notes 1.8 documentation

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply