Programming MIMXRT1060-EVT Board for AN12103

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Programming MIMXRT1060-EVT Board for AN12103

ソリューションへジャンプ
2,776件の閲覧回数
katie
Contributor I

Hi all, 

I'm trying to use the MIMXRT1060-EVT board to run this 

https://community.nxp.com/docs/DOC-342085

application note using the MT9M1114 to create a webcam. 

However, I am running into issues programming the board with this project. 

Here are the errors I'm receiving; 

error1.PNG

error2.PNG

error3.PNG

This is the error reported in the console 

EraseSector (0x60000000, 0x0, 0x1) status 0x40 - driver reports init failure - EXTSPI driver rc -1 (0xFFFFFFFF)
complains because another operation was called after Init failed (status 0x40)

I am using MCUXpresso IDE, using the MIMXRT1060 SDK (2.6.0), in QSPI mode. 

I have cleared the flash memory before running this as well in case of prior "bad" code as suggested in the user manual. 

I have also attempted to follow the instructions in the guide manually to no avail. 

I have been able to program the board with demo code (such as hello_world) so I know that the debug port is in the correct functional mode.

I am running the board off an external power supply, not the USB header. 

Any suggestions would be appreciated! 

ラベル(1)
0 件の賞賛
返信
1 解決策
2,523件の閲覧回数
katie
Contributor I

Hi Kerry, 

I found that switching to an older version of MCUXpresso (10.2.1) solved this error message. Thank you for your help! 

Katie

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,523件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Katie Bradford

  Do you download the code to the flash?

   If yes, please note, the MIMXRT1060-EVK is using the QSPI flash, but the MIMXRT1050-EVKB is using the hyper flash. So you need to modify the const flexspi_nor_config_t hyperflash_config in evkbimxrt1050_flexspi_nor_config.c file which you can find it from evkbimxrt1050_uvc_demo\evkbimxrt1050_uvc_demo\xip

  You need to use this code:

 

const flexspi_nor_config_t qspiflash_config = {
    .memConfig =
        {
            .tag              = FLEXSPI_CFG_BLK_TAG,
            .version          = FLEXSPI_CFG_BLK_VERSION,
            .readSampleClkSrc = kFlexSPIReadSampleClk_LoopbackFromDqsPad,
            .csHoldTime       = 3u,
            .csSetupTime      = 3u,
            // Enable DDR mode, Wordaddassable, Safe configuration, Differential clock
            .sflashPadType = kSerialFlash_4Pads,
            .serialClkFreq = kFlexSpiSerialClk_100MHz,
            .sflashA1Size  = 8u * 1024u * 1024u,
            .lookupTable =
                {
                    // Read LUTs
                    FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0xEB, RADDR_SDR, FLEXSPI_4PAD, 0x18),
                    FLEXSPI_LUT_SEQ(DUMMY_SDR, FLEXSPI_4PAD, 0x06, READ_SDR, FLEXSPI_4PAD, 0x04),
                },
        },
    .pageSize           = 256u,
    .sectorSize         = 4u * 1024u,
    .blockSize          = 256u * 1024u,
    .isUniformBlockSize = false,
};‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

Please try it on your side.

If you still have question about it, please kindly let me know.


Have a great day,
Kerry

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
2,524件の閲覧回数
katie
Contributor I

Hi Kerry, 

I found that switching to an older version of MCUXpresso (10.2.1) solved this error message. Thank you for your help! 

Katie

0 件の賞賛
返信
2,523件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Katie Bradford,

  Thanks for your updated information.

  As I know, the newest MCUXpresso IDE also works, you need to select the correct .cfx which is related to your board external flash.

  Anyway, it's good to hear you already make it works.

  If you still have questions about this topic, please kindly let me know.

If your question is solved, please help me to mark the correct answer, just to close this case, thank you!

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信