Hi,
I'd like to request an option to also get a .dts file out from the Pins tool for the RT series cpu's.
If you use the i.MX8's, you get a .dts for the A53 cores which is great.
But for the M4 co-processor in these as well as the i.MXRT1064, it would be great if the tool could output a .dts that can be used in Zephyr (RTOS)
Hello,
Customers can use Pins Tool for i.MX Application Processors | NXP
It supports i.MX RT devices. And generate pins initialization code examples.
Note, NXP does not support Linux for i.MX RT, so there is no support
for corresponding .dts files.
Regards,
Yuri.
Hi Yuri,
Let me clarify, my request is:
we're not using linux, we're running Zephyr (rtos) that supports .dts (which is a much better option than the .h+.c files)