Pins for i.MX, option to get .dts for Zephyr

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Pins for i.MX, option to get .dts for Zephyr

1,388 Views
dav1
Contributor V

Hi,

I'd like to request an option to also get a .dts file out from the Pins tool for the RT series cpu's.

If you use the i.MX8's, you get a .dts for the A53 cores which is great.

But for the M4 co-processor in these as well as the i.MXRT1064, it would be great if the tool could output a .dts that can be used in Zephyr (RTOS)

Labels (1)
0 Kudos
Reply
3 Replies

1,290 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Customers can use Pins Tool for i.MX Application Processors | NXP 

It supports i.MX RT devices. And generate pins initialization code examples.


  Note, NXP does not support Linux for i.MX RT, so there is no support

for corresponding .dts files.

Regards,

Yuri.

0 Kudos
Reply

1,290 Views
dav1
Contributor V

Hi Yuri,

Let me clarify, my request is:

  • please make pins tool ouput the pin configuration in .dts format for RT series.

we're not using linux, we're running Zephyr (rtos) that supports .dts (which is a much better option than the .h+.c files)

0 Kudos
Reply

1,290 Views
Yuri
NXP Employee
NXP Employee

Hello,

   https://community.nxp.com/thread/516639 

Regards,

Yuri.

0 Kudos
Reply