Parallel LCD Interface with RT1176

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Parallel LCD Interface with RT1176

6,170件の閲覧回数
BasuGouda86
Contributor I

Processor used RT1176,

Parallel Interface using eLCDIF.

LCD Details are given below:

BasuGouda86_0-1657779727307.png

The timing interface is provided as follows:

I am able to generate the 25MHz eLCDIF clock which I am able to verify using the oscilloscope.

 

Here in our LCD we don’t have HSync and VSync signals and the display is dependent on the Data Enable, but when I run the RGB module I am unable to set the DE.

BasuGouda86_1-1657779760023.png

 

0 件の賞賛
返信
6 返答(返信)

6,162件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
I'm afraid that neither eLCDIF nor LCDIF v2 can support the LCD panel without the HSync and VSync signals.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

0 件の賞賛
返信

5,285件の閲覧回数
tbayram
Contributor IV
Hi @jeremyzhou
İs there any update to use DE without HSYNC & VSYNC on eLCDIF or LCDIF v2
0 件の賞賛
返信

6,159件の閲覧回数
Yatish
Contributor I

Dear Jeremyzhou,

Please let us know how do we interface DE mode RGB  LCD .

 

 

Thanks

Yatish.M

 

 

0 件の賞賛
返信

6,137件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
In my opinion, I'd like to suggest you use the FlexIO to connect the LCD panel.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

6,161件の閲覧回数
BasuGouda
Contributor I

Thank you for your quick response,

Is there any way we can use the Parallel RGB LCD display.

As the same LCD is being used with us using the imx6dl processor

Any help is apprecieated.

 

Thank in advance

0 件の賞賛
返信

6,164件の閲覧回数
BasuGouda
Contributor I

Hi,

Please look into the above issue on the interfacing LCD, mistakenly it was sent using the different ID.

Also for your information I tried using the LCD example given in the SDK and changed according to the requirement as suggested in the 

Solved: how to use parallel display interface in I.MXRT117... - NXP Community

Our LCD doesn't have the VSync and HSync interface and hence these pins are not muxed to the LCDIF interface.

Kindly help us out here

Thanks in advance

 

0 件の賞賛
返信