OpenSDA drag&drop to QSPI flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OpenSDA drag&drop to QSPI flash

1,881 Views
bzhang3
Contributor I

The OpenSDA was working for me to load image to HyperFlash on the IMXRT1050-EVKB board. Now I'm switching to QSPI flash. I made the HW mods, updated latest DAP-Link firmware for QSPI (DAPLink v0244 - Supports onboard spi-flash). Now the drag & drop is not working anymore.

Search found this old doc:

i.MX RT1050 CMSIS-DAP drag-and-drop programming | NXP Community 

I ran into the same issue as the user Kent. According to Melissa, "This is a known issue with the latest version of the QSPI DAPLink application. We are working to get an update posted that fixes the problem. In the meantime, I recommend sticking with programming through the IAR IDE."

This was back in June. Does anybody know if this issue is being worked on and ETA?

Thanks,

Bin

 

Labels (1)
0 Kudos
Reply
0 Replies