Not able to program and debug in MIMXRT1170-EVK board using keil and ulink pro.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Not able to program and debug in MIMXRT1170-EVK board using keil and ulink pro.

1,110 Views
Jaga123
Contributor I

Hi,

I am using keil 5.36 ide and ulink prod to download the hex file and debugging. In this evalution board I am not able to load the code. here I attached the error photo. 

Can I able to load the the code with ulink prod or should I follow some other method?

 

 

 

image.pngimage.png

0 Kudos
Reply
5 Replies

1,082 Views
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi,

 

Are you able to flash and debug your board with another debugger and IDE? For instance, using the on-board debugger and MCUXpresso IDE?

 

Regards,

Daniel.

0 Kudos
Reply

1,066 Views
Jaga123
Contributor I
Yes, I am able to flash using on-board debugger and MCUXpresso IDE.
0 Kudos
Reply

1,048 Views
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Thank you for confirming.

Unfortunately, I don’t have a ULINK Pro to test it on my side.

By any chance, have you already reached ARM to ask them about this?

 

Reagrds,

Daniel.

0 Kudos
Reply

1,002 Views
Jaga123
Contributor I
Ok thank you. I will ask them.
0 Kudos
Reply

1,073 Views
Jaga123
Contributor I

For now I don't have any other debugger or ide. My understanding is that this MIMXRT1176 don't have any internal flash so we have to program external flash only. for that any other configuration required?

since I am directly taking examples provided in keil ide and changing only debugger configuration to ulink prod  from cimsis dap and build the code and tried to load . I also tried cimsis dap but same issue I am facing. I may be wrong since I am using this type of board first time.

0 Kudos
Reply