Need the open-source VoIP call service providing software compatible RT600 MCUs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Need the open-source VoIP call service providing software compatible RT600 MCUs

2,863 次查看
bansi_raychura
Contributor II

Hi,

We want to know which are the SIP(Session Initiation Protocol) services providing software(like linphone) that can be used with the i.MX RT600 series for VoIP service.

i.e We are finding an alternative to the linphone that can use with RT600 series MCUs so if there are any, please provide us the name or the source from which we can find them.

Our main purpose is VoIP calls with i.MX RT600 if anything else you have related to it then please provide us.

We are planning to use i.MX RT600 in a voice streaming device for two-way communication, so VoIP call is an important feature for a product please provide any insights if you have any idea.

Thank you in Advance.

0 项奖励
回复
5 回复数

1,277 次查看
Kathrininfanta
Contributor I

For VoIP on the i.MX RT600 series MCU, here are some SIP alternatives to Linphone:

  1. PJSIP: A lightweight, open-source SIP stack ideal for embedded systems. PJSIP Website
  2. Asterisk: A powerful open-source VoIP server that can be adapted for embedded devices. Asterisk Website
  3. FreeSWITCH: An open-source communication platform that supports SIP and is customizable for embedded use. FreeSWITCH Website
  4. Jitsi: Provides open-source VoIP and video conferencing; can be adapted for embedded systems. Jitsi Website
  5. MDev Group SIP Stack: Offers SIP solutions tailored for embedded systems. MDev SIP Stack

For the best results, consider PJSIP for its lightweight nature and good support for ARM-based devices like the i.MX RT600.

0 项奖励
回复

2,829 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @bansi_raychura,

We do not provide VoIP support for the i.MX RT600, specially since this device does not have a dedicated ethernet module. Sorry for the inconvenience this may cause.

 

BR,

Edwin.

2,828 次查看
bansi_raychura
Contributor II
Hi @EdwinHz,

Thanks for reply,

As RT600 have the SDIO interface so we want to use Wi-fi with it, does not VoIP service can be use with the Wi-Fi ?

In research We also found that there is some Conversa voice suite,
we want to know that does conversa voice suite is type of SIP(Session Initiation Protocol) ? or does it include other SIP softwares ?

Does it possible to use i.MX RT600 + Wi-Fi + Conversa voice suite for VoIP service ?

Thanks & Regards
0 项奖励
回复

2,820 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Yes, VoIP can be done via WiFi. However NXP does not provide support of VoIP for the RT600 in any way. Perhaps a custom implementation of this would work, but we cannot guarantee it.

As for the Conversa Voice Suite, we do support it. However, please contact the following email address for more information about its usage and functionality: Voice@nxp.com

 

BR,

Edwin.

0 项奖励
回复

2,839 次查看
bansi_raychura
Contributor II

Hi,

If anyone knows about anything please guide us on what we can do about it.

0 项奖励
回复