Microcontroller/Microprocessor with two USB HS and 16 endpoints

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Microcontroller/Microprocessor with two USB HS and 16 endpoints

2,185 Views
atas2000
Contributor II

Is there a Microcontroller/Microprocessor with two USB HS and 16 endpoints?

0 Kudos
Reply
1 Reply

2,131 Views
FelipeGarcia
NXP Employee
NXP Employee

Hello Aleksandr,

 

The closest recommendation I can give you from the MCU side are RT1050, RT1060 or RT1064. This MCU includes two USB 2.0 Controller Cores that supports up to 8 bidirectional endpoints each.

 

There are other options such as LPC546XX family or LPC5500 family but these MCUs support only one HS USB module and one FS USB module.

 

Have a great day,
Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply