Max camera resolution i.MX RT can support ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Max camera resolution i.MX RT can support ?

2,582件の閲覧回数
hiectai
Contributor III

Hello community.
I have project about camera with i.mx rt 1050, and I need to know about max camera resolution i.mx rt can support ?

I looked at the datasheet and related documents but could not find the answer. Please help me.
Thanks in advance

ラベル(1)
タグ(1)
3 返答(返信)

2,377件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi

It depends in the memory buffer used, speed and pixel format that you want, for example, you could have a 1280×720 8bits/pixel rgb format or a 3840x2160 8bits/pixel monochromatic format.

the SDK package included code with the OV7725 VGA camera sensor 640×480 pixels and the MT9M114 HD camera 1296×976 pixels

Regards

2,377件の閲覧回数
hiectai
Contributor III

Hi Jorge Antonio Alcala Vazquez

Thank you so much.

0 件の賞賛
返信

2,377件の閲覧回数
hiectai
Contributor III

Anybody can help me?

0 件の賞賛
返信