Would it be possible to get an ascii export of the .brd file. This would be an extension .alg. Altium can then import this, but this file can only be created from a Allegro licensed PC.
Regards
Geir Myklatun
Would also be possible to get an ascii export of LAY-31399_C.brd from the 8M MINI EVK LPDDR4 CM_Rev C Customer Release Package?
Hello Chad,
Unfortunately, I have not the information for 8M MINI EVK lPDDR4. Sorry for the inconvenience may cause.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hello,
I provide the reference file via email. Hope it help you.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hello fangfang,
I am still waiting for the ascii export of the .brd file.
Regards
Geir
Hello,
I sent it to your email . Please check it again. Thanks
Hello,
Sorry, but I can’t find I have received an e-mail from you with the design file attached. Can you please try to send it once again?
Regards
Geir
Fra: fangfang <admin@community.nxp.com>
Sendt: tirsdag 23. april 2019 04.17
Til: Geir Myklatun <geir.myklatun@mykes.no>
Emne: Re: - Re: MIMXRT1060-EVK, Design files for Altium Designer
<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg> NXP Community
Re: MIMXRT1060-EVK, Design files for Altium Designer
reply from fangfang <https://community.nxp.com/people/fangfang?et=watches.email.thread> in i.MX RT - View the full discussion <https://community.nxp.com/message/1142340?commentID=1142340&et=watches.email.thread#comment-1142340>
Hello,
I just sent the reference files again. Please check it.
Hi, we urgently require these files also - please can you send to us?
Thanks!!!
Hi fangfang,
Thanks a lot. I'm still waiting for the reference file, but will inform you as soon as I have received it and tried it with the importer.
Regards
Geir