MIMXRT1060 EVB OpenSDA Maintenance Mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MIMXRT1060 EVB OpenSDA Maintenance Mode

843件の閲覧回数
choonshyan_lim
Contributor II

Hi,

Unable to see disk named "MAINTENANCE" in Windows 10 after following the guide listed below for reference.

Have I missed any steps?

My Steps,

1:  5V input not connected

2:  Press SW8 when inserting USB cable

3: Still see disk named "RT1060 EBV"

"For the MIMXRT1060 EVK board, J41 is the connector between the USB host and the RT1060. To update the Open SDA firmaware, press the SW8 and Power on the board. There is a disk named "MAINTENANCE".

Cheers,

Shyan

0 件の賞賛
返信
2 返答(返信)

802件の閲覧回数
choonshyan_lim
Contributor II

Please close this thread.  Press SW9 instead of SW8 would see disk named "MAINRENACE".

0 件の賞賛
返信

802件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi Choon,

 

Thanks for letting us know! I am glad that you could find the issue.

 

Best regards,

Felipe

0 件の賞賛
返信