MIMXRT1060 EVB OpenSDA Maintenance Mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIMXRT1060 EVB OpenSDA Maintenance Mode

841 Views
choonshyan_lim
Contributor II

Hi,

Unable to see disk named "MAINTENANCE" in Windows 10 after following the guide listed below for reference.

Have I missed any steps?

My Steps,

1:  5V input not connected

2:  Press SW8 when inserting USB cable

3: Still see disk named "RT1060 EBV"

"For the MIMXRT1060 EVK board, J41 is the connector between the USB host and the RT1060. To update the Open SDA firmaware, press the SW8 and Power on the board. There is a disk named "MAINTENANCE".

Cheers,

Shyan

0 Kudos
Reply
2 Replies

800 Views
choonshyan_lim
Contributor II

Please close this thread.  Press SW9 instead of SW8 would see disk named "MAINRENACE".

0 Kudos
Reply

800 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Choon,

 

Thanks for letting us know! I am glad that you could find the issue.

 

Best regards,

Felipe

0 Kudos
Reply