MCU-OTA SFW | Cannot generate bin files。

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCU-OTA SFW | Cannot generate bin files。

1,356 次查看
czmyouyu
Contributor I

<MCU-OTA SBL and SFW user guide.pdf>,I follow the following method. but nothing happens,no bin files or errors gengerated。

czmyouyu_0-1642730464877.png

标记 (1)
0 项奖励
回复
3 回复数

1,342 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
非常感谢使用NXP产品,很高兴为你提供技术支持!
谨慎起见,请先介绍一下你的测试环境以便复现问题!!
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

1,333 次查看
czmyouyu
Contributor I

非常感谢回复。

开发环境:Win10     .Keil 5.32

依照《MCU-OTA SBL and SFW user Guide》中7.3.2 Aliyun OTA章节中步骤,依次执行,MDK5.30生成两个bin文件,在执行7.3.2.4 Modify the cur_version for testing的第9步骤时,

python imgtool.py sign --key sign-rsa2048-priv.pem --align 4 --version "1.0.0" --header-size
0x400 --pad-header --slot-size 0x100000 --max-sectors 32 sfw_1064_100.bin 1064_ali_100.bin
python imgtool.py sign --key sign-rsa2048-priv.pem --align 4 --version "1.4.0" --header-size
0x400 --pad-header --slot-size 0x100000 --max-sectors 32 sfw_1064_140.bin 1064_ali_140.bin

并没有相应的bin文件产生,也并没有产生任何的错误log。

 
 

 

0 项奖励
回复

1,318 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,

Thanks for your reply.
你的Python版本是多少?还有你有用IAR工程时会遇到同样的问题吗??
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复