Linux port for i.MX RT boards?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Linux port for i.MX RT boards?

709件の閲覧回数
ronkohen
Contributor I

Hello,

Does anybody know of Linux ports to i.MX RT boards, IMXRT1170 in particular?

Thanks!

Ron

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

670件の閲覧回数
sergeiposelenov
Contributor I

Indeed, Emcraft develops and supports Linux (uClinux) BSPs for various i.MX RT SoCs, including the i.MX RT 1170.

 
Key features of the BSPs are as follows:
 
- Linux kernel v 6.1.22, which is the same kernel baseline NXP currently supports for the MMU-full SoCs (eg. i.MX 8M*, etc). Basically, it means you have the latest Linux kernel, with all I/O stacks, device drivers, etc running on the i.MX RT.
 
- Various I/O device drivers and stacks (eg. Linux TCP/IP stack, UBIFS on Flash, CANsocket, ADC, USB Host and Gadgets, LVGL Graphics, WiFi/BT, GPIO, I2C, SPI, etc)
 
- Recent GNU toolchain (GCC 11.3.0) optimised for Cortex-M7 
 
- Support for ELF and shared libraries
 
- Hardware FPU enabled.
 
We provide a Linux demo tailored for the NXP i.MX RT EVK boards. See, for instance: 
 
0 件の賞賛
返信

698件の閲覧回数
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

You can consult with our partner Emcraft Systems LLC, which develops uClinux BSPs for some of our boards, IMXRT1170 is included.

Hope it helps you.

Have a nice day!

0 件の賞賛
返信