LPSPI1 Not Receiving data on MIMXRT1170EVKB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPSPI1 Not Receiving data on MIMXRT1170EVKB

Jump to solution
2,035 Views
matt55354
Contributor II

I'm using the MIMXRT1170EVKB dev board and attempting to read/write SPI data from the MX25L4006 flash over LPSPI1.  

Problem: I can see data being sent to the flash (0x5a RDSFDP instruction) over SOUT, and I can see correct data returning from from the flash(on SIN), and the FIFO count(FSR_RXCOUNT) increments correctly, but the data from RDR_DATA ALWAYS reads 0. (the data on the physical line is NOT 0)

GPIO_AD_31Mux is set to 0 (LPSPI_SDI), and pad settings are default(0x6 on SW_PAD_CTL_PAD_GPIO_AD_31)

I'm confident clock phase and polarity are correct, since the data on the SIN line when decoded off the scope is the expected SFDP Signature( 0x53464450).  

Other tidbits:  I set SIN to a gpio, polling the level during a transaction, and was able to see the line changing the correct number of pulses, eliminating a suspicion of an unsoldered pad under the RT1176.

At this point, I'm suspecting an errata or a datasheet error.  Any help would be appreciated!

Also, I attached a scope trace showing SCK, SIN, and SOUT.

0 Kudos
Reply
1 Solution
1,938 Views
matt55354
Contributor II

For posterity, the solution was that LPSPI1_LPSPI_SDI_SELECT_INPUT daisy chain was not set to point to pin GPIO_AD_31.  After finding this, everything is working as expected.  Thanks to Ramdas Chary from Arrow Electronics for the hint on this.

View solution in original post

0 Kudos
Reply
4 Replies
1,939 Views
matt55354
Contributor II

For posterity, the solution was that LPSPI1_LPSPI_SDI_SELECT_INPUT daisy chain was not set to point to pin GPIO_AD_31.  After finding this, everything is working as expected.  Thanks to Ramdas Chary from Arrow Electronics for the hint on this.

0 Kudos
Reply
1,962 Views
matt55354
Contributor II

Just to be thorough, I'm attaching the scope shot with#cs0. 

tek00004.pngtek00004.png

0 Kudos
Reply
1,974 Views
matt55354
Contributor II

Yes, I've previously verified CS# is functioning.  This is apparent from the scope trace as the correct data is being returned from the chip on SIN.  The problem is that reading RDR_DATA always returns 0.

0 Kudos
Reply
1,997 Views
mayliu1
NXP Employee
NXP Employee

Hi @matt55354 ,

Thank you so much for your interest in our products and for using our community.

I check your post  about a scope trace showing SCK, SIN, and SOUT, but without SPI_PCS signal.

Could you please check LPSPI1_PCS0 signal by using a scope.

mayliu1_1-1749180747431.pngmayliu1_1-1749180747431.png

I search MX25L4006E datasheet for you, I find it describe that "When the device is not in operation and CS# is high, it is put in standby mode."

mayliu1_0-1749180642867.pngmayliu1_0-1749180642867.png

Wish it helps you.
If you still have question about it, please kindly let me know.

Wish you a nice day!

Best Regards
MayLiu

0 Kudos
Reply