Is there any errata regarding MIPI_CSI2 RX Controller supported data format?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there any errata regarding MIPI_CSI2 RX Controller supported data format?

2,181件の閲覧回数
burhanhagi
Contributor V

I re-checked the MIPI-CSI2 Peripheral in IMX Reference Manual. In below screenshots, there is no sign that CSI2 RX Controller supports ITU-R.BT656 protocol or not. However it supports YUV422 and RGB565 data formats and other RGB/YUV different bit combinations.

burhanh_0-1678372919199.png

burhanh_1-1678372975989.png

As I mentioned in other ticket does imxrt1170 MIPI-CSI2 peripheral support serial itu-r.bt656 format? 

ADV7280-M sends active YUV422 video data within a form of ITU-R.BT656 protocol packet inside. Here is the ITU-R.BT656 format structure.

burhanh_0-1678426902219.png

So I suspect that MIPI CSI2 RX Controller is not even aware of ITU 656 format. That is why I could not get video from adv chip. Waiting your thoughts/recommendations.

 

タグ(3)
0 件の賞賛
返信
2 返答(返信)

2,077件の閲覧回数
burhanhagi
Contributor V

Hi @jingpan, 

At last, I am now able to run ADV7280M with NXP IMXRT1176. I can get live video over it. My above post is actually wrong.

ADV7280M actually gives its output as YUV422. MIPI CSI data format and  ITU-R.BT656 format is totally different.

In order to run ADV7280-M MIPI CSI, one must run NXP IMXRT CSI peripheral in CSI gated clock mode with HSYNC active HIGH. 

0 件の賞賛
返信

2,117件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @burhanhagi ,

Yes, it doesn't support BT656.

 

Regards,

Jing

0 件の賞賛
返信