Hi,
I'm using i.MX RT1170 EVK kit.
Is NXP support uClinux for i.MX RT1170 EVK?
My requirement is to transfer the camera data from device to host through ethernet. I tried in bare-metal OS and I can't able to achieve the maximum ethernet throughput from Iperf RX TX test.
Hoping for better guidance.
Thanks and Regards,
Bala
Solved! Go to Solution.
Hello Bala,
I would recommend contacting Emcraft support regarding this issue to see if they may provide more details on what could be causing it.
My apologies for the inconvenience.
Regards,
Gustavo
Hi Gustavo,
I tried the default uCLinux package from emcraft, in that package 100Mbps Ethernet only working 1Gbps is not working.
Boot log:
/ # Micrel KSZ8081 or KSZ8091 40424000.etherne:02: attached PHY driver [Micrel KSZ8081 or KSZ8091] (mii_bus:phy_addr=40424000.etherne:02, irq=-1) |
Thanks & Regards,
Bala
Hello Bala,
I would recommend contacting Emcraft support regarding this issue to see if they may provide more details on what could be causing it.
My apologies for the inconvenience.
Regards,
Gustavo
Hello Bala,
NXP foes not provide uClinux support for the i.MXRT1170 EVK. However, there is a uClinux BSP from Emcraft (link below) which is maintained and supported by them.
https://www.emcraft.com/imxrt1170-evk-board
I hope that this information helps.
Regards,
Gustavo