Is NXP support uClinux for i.MX RT1170 EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is NXP support uClinux for i.MX RT1170 EVK

Jump to solution
2,334 Views
balasubramaniyam
Contributor II

Hi,

I'm using i.MX RT1170 EVK kit.

Is NXP support uClinux for i.MX RT1170 EVK?

My requirement is to transfer the camera data from device to host through ethernet. I tried in bare-metal OS and I can't able to achieve the maximum ethernet throughput from Iperf RX TX test.

Hoping for better guidance.

Thanks and Regards,

Bala

Tags (1)
0 Kudos
Reply
1 Solution
2,292 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Bala,

I would recommend contacting Emcraft support regarding this issue to see if they may provide more details on what could be causing it.

My apologies for the inconvenience.

Regards,
Gustavo

View solution in original post

0 Kudos
Reply
3 Replies
2,305 Views
balasubramaniyam
Contributor II

Hi Gustavo,

I tried the default uCLinux package from emcraft, in that package 100Mbps Ethernet only working 1Gbps is not working. 

Boot log:

/ # Micrel KSZ8081 or KSZ8091 40424000.etherne:02: attached PHY driver [Micrel KSZ8081 or KSZ8091] (mii_bus:phy_addr=40424000.etherne:02, irq=-1)

 

Thanks & Regards,
Bala

0 Kudos
Reply
2,293 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Bala,

I would recommend contacting Emcraft support regarding this issue to see if they may provide more details on what could be causing it.

My apologies for the inconvenience.

Regards,
Gustavo

0 Kudos
Reply
2,322 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Bala,

NXP foes not provide uClinux support for the i.MXRT1170 EVK. However, there is a uClinux BSP from Emcraft (link below) which is maintained and supported by them.

https://www.emcraft.com/imxrt1170-evk-board

I hope that this information helps.

Regards,
Gustavo

0 Kudos
Reply