Is MIMXRT1021CAF4A Digital Input 5V Tolerant?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is MIMXRT1021CAF4A Digital Input 5V Tolerant?

ソリューションへジャンプ
862件の閲覧回数
ergingursoy
Contributor I

Hi,

Is digital inputs are 5V tolerant? I looked at the reference manual and datasheet but could not find any info about it.

Regards

#iMXRT1021

0 件の賞賛
返信
1 解決策
852件の閲覧回数
diego_charles
NXP TechSupport
NXP TechSupport

Hi @ergingursoy 

I hope that you are doing great!

No, digital pins  or GPIO pins  are not 5V tolerant. 

RT1021 GPIOS can work with  1.8v or 3.3v nominal voltage.

For example , If we still want to know the maximum input  voltage GPIOs  can tolerate, we can take a look at the below specification.

diego_charles_0-1655917993381.png

The maximum input voltage of input pins is limited to  maximum of the NVCC_GPIO rail. 

diego_charles_1-1655918003922.png

All the best, 

Diego

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
853件の閲覧回数
diego_charles
NXP TechSupport
NXP TechSupport

Hi @ergingursoy 

I hope that you are doing great!

No, digital pins  or GPIO pins  are not 5V tolerant. 

RT1021 GPIOS can work with  1.8v or 3.3v nominal voltage.

For example , If we still want to know the maximum input  voltage GPIOs  can tolerate, we can take a look at the below specification.

diego_charles_0-1655917993381.png

The maximum input voltage of input pins is limited to  maximum of the NVCC_GPIO rail. 

diego_charles_1-1655918003922.png

All the best, 

Diego

 

0 件の賞賛
返信