Interfacing 24 bit TFT to iMXRT1062 using LVDS transmitter+Ethernet+EMC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Interfacing 24 bit TFT to iMXRT1062 using LVDS transmitter+Ethernet+EMC

431 Views
EmbeddedTech
Contributor III

Hi,

I am using iMXRT1062 and will be using the LVDS transmitter DS90C385AMT to connect to the 24 bpp 7"display . We also need to use the Ethernet and the EMC controller for SDRAM. Since Ethernet shares the LCDIF pins (or SDRAM pins), some of the RGB lines required for the LCD uses the GPIO pins. How to use the eLCDIF controller to send data if not all 24 lines are eLCDIF pins? Is there any alternate solution for Ethernet without disturbing the LCD and SDARM pins?

Your help on this is highly appreciated.

0 Kudos
Reply
0 Replies