Integrity check

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Integrity check

744 次查看
Deviprasad
Contributor I

Hi,

    I am using i.MX RT1176 with SPI FLASH(W25Q16JVUX)for my application . I want to integrity check for the system(Flash, RAM and CPU etc). Please guide me to do.

0 项奖励
回复
1 回复

714 次查看
mayliu1
NXP Employee
NXP Employee

Hi @Deviprasad ,

 

Thank you so much for your interest in our products and for using our community.

Question:  I want to integrity check for the system(Flash, RAM and CPU etc). Please guide me to do.

Answer: 

1: For Flash,  I suggest you can use SDK demo "evkbmimxrt1170_flexspi_nor_polling_transfer_cm7", and link application to RAM.

mayliu1_0-1746585415687.png

In this example, flexspi will send data and operate the external Nor flash connected with FLEXSPI.

2: For RAM,  I suggest you can refer to application Note 

https://www.nxp.com.cn/docs/en/application-note/AN12077.pdf

i.MX RT1170 ECC Application

I do not suggest you burn Fuse to enable ECC  for test.

3: For CPU and Peripherals:

I suggest you can run SDK demo on your board.

NXP releases a lot of SDK demos, you can refer to.

https://mcuxpresso.nxp.com/en

Wish it helps you.
If you still have question about it, please kindly let me know.

Wish you a nice day!

Best Regards
MayLiu

0 项奖励
回复