IMXRT1180 Memory debugging RW error or encry?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMXRT1180 Memory debugging RW error or encry?

779 Views
Haoxxxxxxxx
Contributor I

When debugging the MIMXRT1180-EVK board, if there are some errors in the program, the mcu seems to predict in advance and cause undetectable memory read and write errors (such as the function stack) that can't be debugged. Especially on OCRAM memory and HYPERRAM, even if the program is running properly, JLINK still cannot read out the correct value in memory. Including the Keil routine in the SDK will also appear, is this an IMXRT1180 encryption method? How do I get JLINK and OCRAM/HYPERRAM memory to work?

0 Kudos
Reply
1 Reply

697 Views
Sam_Gao
NXP Employee
NXP Employee

Hi 

IMXRT1180 EVK board is not yet available to the public, it only for beta key customers with dedicated channel both hardware and software, please contact you local FAE or sales for help, pleas feel free to tell us if you have any questions.

0 Kudos
Reply