IMXRT1064 FLEXSPI Hyper Flash Pooling Transfer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMXRT1064 FLEXSPI Hyper Flash Pooling Transfer

1,650 Views
Lukas_Frank
Senior Contributor I

Hi Dear Authorized,

 

I am trying to use an external nor flash on my card. I am successfully able to writing into it. But I am getting  error for “kStatus_FLEXSPI_SequenceExecutionTimeout” in FLEXSPI_CheckAndClearError method during FLEXSPI_ReadBlocking operation.

 

Could you please help me about it?

 

Thanks and Regards.

0 Kudos
Reply
3 Replies

1,636 Views
RaRo
NXP TechSupport
NXP TechSupport

Hello @Lukas_Frank,

Just to confirm, are you using a custom board or is it an EVK from NXP? If is an EVK, which one do you have (EVK or EVKB)?

Also, which NOR Flash are you using?

Best regards, Raul.

1,626 Views
Lukas_Frank
Senior Contributor I

Hi Dear @RaRo ,

 

I am using my custom board. It includes S26KS512SDPBHV020. I just want to use my DRAM and NOR Flash memories in board. But I have implementation problems with both them.

 

Best wishes.

0 Kudos
Reply

1,611 Views
RaRo
NXP TechSupport
NXP TechSupport

Hello @Lukas_Frank,

Just for double check, are you testing the SDK example: flexspi_hyper_flash_polling_transfer? If so, did you modify something in the code? What have you modified?

Also, if you are using the example could you please send us a picture of what is displayed at the terminal?

Have you tried this issue on one of our boards (EVK or EVKB)? Is the issue there too?

If you are not using the SDK example nor have one of our boards (EVK or EVKB) for test, can you share a demo that we can use to replicate the issue?

Best regards, Raul.

0 Kudos
Reply