IMXRT102XSRM - Fuse map discrepancies.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMXRT102XSRM - Fuse map discrepancies.

1,484件の閲覧回数
rshipman
Contributor V

Hi,

I found some fusemap discrepancies in the manual:

Security Reference Manual for the i.MX RT102x Processor
IMXRT102XSRM
Rev. 0, 07/2020

#### Problem 1:

In tables 4-2 to 4-7, we have these settings:

0x470[1] L1 D-Cache DISABLE
0x470[20] Reserved
0x470[23] USDHC_CMD_OE_PRE_EN
0x470[30:24] MMC_DLL_DLY[6:0]

But in Table 4-9. Fusemap Descriptions, these are different:

0x470[1] BT_MPU_DISABLE
0x470[20] BT_LPB_POLARITY
0x470[23] Reserved
0x470[30:24] MMC_DLL_DLY[6:0]  Setting field differs: "Conneted to LVDS module."

Which ones are correct please?
Similar problems seem to appear in manuals:
i.MX RT1020 Processor Reference Manual, Rev. 2, 01/2021
i.MX RT1050 Processor Reference Manual, Rev. 3, 8/2019


#### Problem 2:

In Table 4-9. Fusemap Descriptions, fuses 0x460[7:6] seem to be described twice:

0x460[6] Reserved
0x460[7] Reserved
0x460[7:6] FLASH_CONNECTION_SEL

Which ones are correct please?


Many thanks and kind regards,
Ronnie

ラベル(1)
タグ(3)
0 件の賞賛
返信
5 返答(返信)

1,451件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi Ronnie,

I have received confirmation from internal team. Please check it below:

  • For issue #1, 0x470[1] BT_MPU_DISABLE, etc. in Table 4-9. Fusemap Descriptions is correct for RT10xx . Doc team will fix the corresponding part in table 4-2 to 4-7.
  • For issue #2,  0x460[7:6] Reserved  is correct for RT10xx. 

Thank you for bringing this to our attention.

Best regards,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time. 

------------------------------------------------------------------------------ 

0 件の賞賛
返信

1,440件の閲覧回数
rshipman
Contributor V

Hi Felipe,

Thanks for your reply.

Regarding issue #1:

Unfortunately what you said about BT_MPU_DISABLE seems to contradict this posting: https://community.nxp.com/t5/i-MX-RT/RT1020-RT1050-ref-manual-issue-BT-MPU-DISABLE-and-L1-I-Cache/m-...

Also, I just want to confirm that all the settings in #1 are correct in table 4-9 (and incorrect in the other tables)?

Kind regards,

Ronnie

 

 

 

0 件の賞賛
返信

1,387件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi Ronnie,

Sorry for the late reply, I have confirmed with my colleague and with internal team that the information from my previous reply is correct.

Best regards,

Felipe

0 件の賞賛
返信

1,363件の閲覧回数
rshipman
Contributor V

Thank you.

0 件の賞賛
返信

1,468件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi Ronnie,

Thank you for reporting this with us. I am going to check internally and I will update this thread when I receive confirmation about this.

Best regards,

Felipe

0 件の賞賛
返信