Hi,
In the manual:
i.MX RT1020 Processor Reference Manual, Rev. 1, 12/2018
Table 21-9. Fusemap Descriptions
Page 1116
The table specifies:
0x470[1] BT_MPU_DISABLE
0x470[2] L1 I-Cache DISABLE
However in the tables:
Table 21-2. FlexSPI (Serial NOR) boot fusemap, page 1098
Table 21-3. SD boot fusemap, page 1100
Table 21-4. MMC/eMMC boot fusemap, page 1102
Table 21-5. SEMC (NAND) boot fusemap, page 1103
Table 21-6. SEMC (NOR) boot fusemap, page 1105
Table 21-7. FlexSPI1 (Serial NAND) boot fusemap, page 1106
The tables show:
0x470[1] L1 D-Cache DISABLE
0x470[2] L1 I-Cache DISABLE
So what does 0x470[1] actually do?
The same issue exists in the RT1050 Reference Manual as well, so if this is a mistake, it might be worth checking the RMs of all similar devices:
i.MX RT1050 Processor Reference Manual, Rev. 3, 8/2019
Kind regards,
Ronnie
Hello,
0x470[1] L1 D-Cache DISABLE
0x470[2] L1 I-Cache DISABLE
Should be correct. Thanks for your feedback and we will forward it to the related team.
Have a nice day.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------