IMXRT1024 LPUART FIFO Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMXRT1024 LPUART FIFO Issue

3,763 Views
Lukas_Frank
Senior Contributor I

Hi all,

I'm setting the LPUART FIFO RX and TX sizes and it only seems to be 4 words and cannot be set to any other value.  In the RM it says maximum number of receive or transmit fifo size data word can be up to 256 words. 

 

I have examine the following register:


Parameter Register (PARAM)

LPUART FIFO Register (FIFO)

LPUART Watermark Register (WATER)

But nothing is work to set my FIFO size..

 

How can I set it manually?

Why do you write, from 1word to 256word, on RM like a size-scale for FIFO if I am not able to use that size?

 

Thanks and Regards.

0 Kudos
Reply
5 Replies

3,759 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi @Lukas_Frank :

From the source code, you can configure the FIFO size the before LPUART_INIT function

/*
* config.baudRate_Bps = 115200U;
* config.parityMode = kLPUART_ParityDisabled;
* config.stopBitCount = kLPUART_OneStopBit;
* config.txFifoWatermark = 0;
* config.rxFifoWatermark = 0;
* config.enableTx = false;
* config.enableRx = false;
*/
LPUART_GetDefaultConfig(&config);
config.baudRate_Bps = BOARD_DEBUG_UART_BAUDRATE;
config.enableTx = true;
config.enableRx = true;

 

config.txFifoWatermark = your size;

config.rxFifoWatermark = youe size;

LPUART_Init(DEMO_LPUART, &config, DEMO_LPUART_CLK_FREQ);

 

Regards

Daniel

0 Kudos
Reply

3,743 Views
danielchen
NXP TechSupport
NXP TechSupport

Sorry, I made a mistake here, watermark is not FIFO size.

 

Please refer to LPUART FIFO register for FIFO size.

danielchen_0-1629794582818.png

 

danielchen_1-1629794605355.png

 

You can configure this register for FIFO size.

 

Regards

Daniel

 

0 Kudos
Reply

3,731 Views
Lukas_Frank
Senior Contributor I

Dear @danielchen Hi again,

 

I set it, but there was no action more than 4 word. Also RM is spesified that this field is read only. When I set RXFIFOSIZE to 256, it still returns RXCOUNT as 4 word maximum. I am just trying to measure what is the size of incoming bytes. What is the truth about FIFO?

Lukas_Frank_0-1629873691603.png

Lukas_Frank_2-1629873764051.png

 

Could you please also view my other question?

Question Get Send/Receive Data Count 

 

Thanks and Regards.

0 Kudos
Reply

3,645 Views
danielchen
NXP TechSupport
NXP TechSupport

 

Sorry, I confirmed with hardware team,  The RXFIFO size is 4 data words.  It is a fixed value, a hardware attribute, not configurable.

 

Regards

Daniel

0 Kudos
Reply

3,754 Views
Lukas_Frank
Senior Contributor I

Hi @danielchen,

 

I set it, but there was no action more than 4 word. There is an assert rule in LPUART_Init. So I am not able to set my FIFO size more than 4. But in reference manual it is read-only form from 1word to 256word. What is the actual size of this FIFO? I indicate that in my question why do not you choose not to answer it ? 

Could you please view my other question? Question Get Send/Receive Data Count 

 

Thanks and Regards.

0 Kudos
Reply