IMXRT 1064 eMMC interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMXRT 1064 eMMC interface

ソリューションへジャンプ
4,063件の閲覧回数
vasudhevan
Contributor V

HI,

   We going to interface 8 bit data line emmc(SDINBDG4-8G) to  uSDHC1 4 bit data line for our application data storage purpose.

   SDINBDG4-8G eMMC 5.1 specification but 1064 supports v4.5/4.2/4.3/4.4/4.41/ this interface will work (or) we need to choose another emmc part number ?

Thanks & Regards

       Vasu

ラベル(1)
0 件の賞賛
返信
1 解決策
3,924件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello

 The EMMC 4.5 or EMMC 5.0 /5.1 is backward-compatible with eMMC4.4, we can use it in eMMC4.4 mode to enable eMMC4.4 functionality and performance on the i.MXRT platform. Booting from an eMMC 4.5 device or higher version is not supported,  boot ROM will fall back to the eMMC4.4
standard when a eMMC4.5 or higher version capable device is detected. That's to say. One  can use eMMC 5.x card. But it will work in eMMC 4.4 mode. Have a nice day.

Best Regards

 

元の投稿で解決策を見る

3 返答(返信)
3,228件の閲覧回数
morphee909
Contributor I

I plan to interface the same EMMC to an RT1064. The EMMC is 5.1 HS400 but the RT1064 is max HS200. So it needs to change clock frequency ? If it is the case does someone knows how to do that ?

0 件の賞賛
返信
3,925件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello

 The EMMC 4.5 or EMMC 5.0 /5.1 is backward-compatible with eMMC4.4, we can use it in eMMC4.4 mode to enable eMMC4.4 functionality and performance on the i.MXRT platform. Booting from an eMMC 4.5 device or higher version is not supported,  boot ROM will fall back to the eMMC4.4
standard when a eMMC4.5 or higher version capable device is detected. That's to say. One  can use eMMC 5.x card. But it will work in eMMC 4.4 mode. Have a nice day.

Best Regards

 

3,924件の閲覧回数
vasudhevan
Contributor V

Hi fangfang,

    Thank you for your response.

     We going to use only data storage purpose.

Thanks & Regards 

       Vasu 

0 件の賞賛
返信