IMX RT 1064 with sdram interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX RT 1064 with sdram interface

ソリューションへジャンプ
2,710件の閲覧回数
vasudhevan
Contributor V

Hi,

   We going to interface 8 bit sdram (AS4C32M8SA-7TCNTR) this part supports imxrt 1064 ?

   What are important pins we needs to concentrate 8 bit sdram interface ?

Thanks & Regards

       Vasu

ラベル(1)
0 件の賞賛
返信
1 解決策
2,554件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello,

The part number is Ok for the Design.

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
2,554件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello,

 The RT1064 supports 8bit SDRAM. Due to I have not the datasheet for the part number AS4C32M8SA-7TCNTR. I can't find the feature for it. Please consider the pins like this when connect to the SRRAM.

pastedImage_1.png

And One may refer to the related information of the  EVK board.

  

Best Regards

0 件の賞賛
返信
2,554件の閲覧回数
vasudhevan
Contributor V

Hi fangfang,

        SDRAM DQS DQS pin should be floating it's mandatory ?

        We using two ethernet.

        Ethernet2 MDIO muxed with GPIO_EMC_39.

        Ethernet2 MDIO one more pin muxed with LCD_ENABLE we using lcd also.

        Now how can i handle DQS pin ?

        

Thanks & Regards

        Vasu

        

0 件の賞賛
返信
2,554件の閲覧回数
vasudhevan
Contributor V

Hi fangfang,

     EVK contains 16bit SDRAM interface.

     Please see attached link datasheet available and give feedback.

     AS4C32M8SA-7TCNTR

Thanks & Regards

       Vasu

0 件の賞賛
返信
2,555件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello,

The part number is Ok for the Design.

0 件の賞賛
返信
2,554件の閲覧回数
vasudhevan
Contributor V

Hi.

  Thank you fangfang

0 件の賞賛
返信