Hi, I'm very new with the nxp rt1060 and with embbeded systems in general. I would like to implement a simple program to route tdm or I2S from the codec CS42448 to the MCU and viceversa. I know there are examples on the sdk and I'm working with them. My problem is that I don't see which files do I need to modify in order to route inputs and outputs. I would be very grateful if someone could give me some help or advices.
I'm using the MIMXRT1060-EVKB and the AUD-EXP42448 audio board.
Thanks in advance
Hi @HeritageMarco ,
You should config pin first. It's in BOARD_InitPins(). You can refer to sai_edma_record_playback. It use SAI1 to record and playback. All things are defined in the top of sai_edma_record_playback.c.
Regards,
Jing
Hi @jingpan, thanks for your answer. I'm trying to understand how SAI and TDM are managed in the example you mentioned. Can you confirm that both frames are structured as these pictures? I found them on google but since there are not related with the MIMXRT1060-EVKB and the AUD-EXP-42448 I'm not 100% sure that both frames work like this.