Using one MDIO signal for both MACs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using one MDIO signal for both MACs

Jump to solution
1,053 Views
jautry
Contributor IV

Since there appears to be a conflict in using ENET2 MDIO signal on GPIO EMC-39 with QSPI.  Is it possible to use the same MDIO signal for both MACs if I want separate LANs for gateway purposes?

Tags (1)
0 Kudos
Reply
1 Solution
1,045 Views
mjbcswitzerland
Specialist V

Hi

The MDIO bus can address 31 different PHYs and the PHYs can be connected to any ENET controller.

Therefore if you have a design using 2 x ENET, each with its own PHY, the two PHYs can be controlled via a single MDIO interface, thus freeing up one of the 2 MDIO buses for other MUX usage.

Regards

Mark

P.S. Search the forum for other posts discussing the same topic and confirming the solution.

View solution in original post

0 Kudos
Reply
1 Reply
1,046 Views
mjbcswitzerland
Specialist V

Hi

The MDIO bus can address 31 different PHYs and the PHYs can be connected to any ENET controller.

Therefore if you have a design using 2 x ENET, each with its own PHY, the two PHYs can be controlled via a single MDIO interface, thus freeing up one of the 2 MDIO buses for other MUX usage.

Regards

Mark

P.S. Search the forum for other posts discussing the same topic and confirming the solution.

0 Kudos
Reply