I.mxrt1170 and software/IDE stability

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.mxrt1170 and software/IDE stability

2,077 Views
simongornall
Contributor I

I'm investigating the i.mxrt1170 as an alternative to the STM32 range (faster, more memory, better chip layout, more ports, etc.) 

The hardware looks excellent for the purpose I have in mind, but I've spent the last two weeks or so not really getting very far with the IDE. 

  • The first time, I naively tried to create a project with all the things I wanted enabled. I've done this before with the STM32CubeMX and it (pretty much) worked. I enabled ethernet, USB (both), SD, LCD, a few SPI/I2C etc. It wouldn't compile - ok, maybe I need to ease into it a bit...
  • Next I tried a 'C' project just to blink an LED, that worked great. 
  • Next I tried a 'C' project with FreeRTOS, that didn't work, but there was an example design I could use, so I thought "ok"
  • Next I tried adding the example 'C' project that uses an SD card with the FreeRTOS design, and that worked as well. I was feeling confident and on a roll! That was 2 weeks ago.

There was no C++ SD-card/FreeRTOS example, so I tried creating a C++ project that implemented these - this is going to be a larger design, so I want the maintainability and data-isolation of C++. This hasn't worked for me. The config I tried is below (steps 1 and 2) in case there's something glaringly wrong...

cfg-step1.png

cfg-step2.png

When the project has finished being made, it refuses to compile due to a conflict in the 'osa' component. There's a "_bm" (bare metal ?) as well as an "_freertos" instance.

Deleting the "fsl_osa_abstraction_bm.*" files in the osa component seems to let it compile, and indeed this then prints out "Hello World" on the console.

So far so good, maybe, but then I tried using the code from the 'C' example, in this C++ project. After fixing up all the make-a-filesystem variables/definitions and altering a few things:

  • Need to get rid of the extra BOARD_SD_Pin_Config() function in board.c
  • Need to change the CD detect algorithm to be DATA3 because the GPIO default doesn't work on the board

... it still didn't work. The SD card code is hanging inside some event-based loop that I don't really understand when it tries to initialise the card.

I'm kind of scared that if it's this hard to get something basic like an SD card working, it's going to be very hard to start integrating all the other peripherals, and I don't want to be in the position where I've invested 3 months of work before hitting a brick wall with (say) ethernet... 

I also noticed that the file structure was a bit different for the example and the SDK-generated code (the newly-generated code puts sdmmc_config.{c,h} into a 'template' directory (which gets compiled, it's not just a template) whereas the example has it under the 'board' subdirectory.

So, am I barking up the wrong tree ? Is it possible to get C++, FreeRTOS, and peripheral code to work well together ?

As another option, I tried last night to use the Azure SD card example. That just hung after initialising the application - no threads appeared to be running... [sigh]

 

 

0 Kudos
Reply
3 Replies

1,982 Views
simongornall
Contributor I

So I tried the guide, and depending on which library I linked against (newlib / new lib-nano etc) got linker errors (it was looking for things like _exit and _getpid (!) which were presumably called from library code) or it just didn't run.

I tried the "new C++ project" approach again, added in the SD card code, added in the pin definitions, changed the GPIOs used to be those from the example code, and .... it still didn't work. I found this answer in the forum, which led me to realise I hadn't initialised the MPU in the startup code, whereas the example code did. 

Called Board_ConfigMPU() at the top of main() and I now have a C++ FreeRTOS task that can format the SD card and create a directory - and I verified that my Mac can read the resulting formatted card  

So it looks as though it was the MPU that was causing me problems... 

0 Kudos
Reply

1,968 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @simongornall,

I'm glad you were able to find the issue and get the task to format and write on the SD card. Please let me know if you have further inquiries about this topic. c:

BR,
Edwin.

0 Kudos
Reply

2,019 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @simongornall,

I'm sorry you're experiencing these difficulties to get going on developing your applications using the RT1170. It should be possible to create a project based on C++ with FreeRTOS and peripheral code working together. You mentioned that you got the FreeRTOS SD example working on your RT1170, so let's start with that and convert it to C++.

The following blog post from a fellow NXPer Erich Styger does a great job describing how to convert a C project to a C++ one in MCUXpresso, so please make sure to follow this guide and implement it for the SD example:

https://mcuoneclipse.com/2020/07/11/from-c-to-c-converting-eclipse-c-projekts/

Do let me know if it helps, or any other difficulties you encounter when following the guide.

BR,
Edwin.

0 Kudos
Reply