I.mx1020 based resources?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I.mx1020 based resources?

822 次查看
sanketkulkarni
Contributor III

I am working on imx1020 for number plate recognition security system. Any resources on this, so that I can get familiar with the imx1020 family till board arrives.

Also any suggestions  on complex project which I can built with imx 1020 which I can present in my CV in future?

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

761 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Sanket kulkarni ,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
From the perspective of performance, the i.MX RT 1020 is able to be used in the number plate recognition security system.
About a similar solution or project demo, there are some neural network demos in the SDK library, these demos demonstrate the i.MX RT can implements classification work, hope they're helpful to you.
SDK library: https://mcuxpresso.nxp.com/en/welcome

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复