How to set the flash driver as default? Loading Flash failed.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to set the flash driver as default? Loading Flash failed.

1,508 次查看
NVazquez
Contributor IV

When I try to load the code I get a fault, "Load failure: Ef(11). No Flash configured".

The sample project flashes fine. The project I created, when I try to load that, I get this fault.

 

The project that flashes have the Default Flash driver setting as this,

Nhule_0-1634750510348.png

 

My project's(Which doesn't flash) GUI Flash Tool looks like this,

Nhule_1-1634750562991.png

Also in my project folder I have two folders missing,  ".mcuxpressoide_packages_support" and  ".metadata". Not sure if it has anything to do with the flash fault.

 

0 项奖励
回复
1 回复

1,500 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Firstly, I'd like to suggest you click the small icon on the down-left corner to gain the error indication, next, I was wondering if you can introduce the steps of creating your project.

jeremyzhou_0-1634796469777.png

Have a great day.
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 项奖励
回复