Hi community ,
Is there any way we can import a middlewear example in the IDE ?
I want to import the MCU Boot middleware .
Or I should have a base templet and manually add the src and include files in the project ?
Thanks and regards ,
Naren Chandra .
解決済! 解決策の投稿を見る。
Hi Naren chandra,
Please read Getting Started with MCUXpresso SDK for EVK-MIMXRT1020.pdf under the SDK path:
SDK_2.7.0_EVK-MIMXRT1020\docs
Then you can follow it to import the bootloader code to the MCUXpresso IDE:
If you still have questions about it, please kindly let me know.
Wish it helps you!
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi Naren chandra,
You can refer to the flashloader project:
SDK_2.7.0_EVK-MIMXRT1020\boards\evkmimxrt1020\bootloader_examples\flashloader
This project is using the middleware:
Wish it helps you!
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi Kerry ,
I am using MCUXpresso , I want to import the bootloader project inside middlewear -> mcu_boot -> bootloader .
The example you share is IAR based , just guide me in importing the project in mcuxpresso .
Thanks and regards ,
Naren Chandra
Hi Naren chandra,
Please read Getting Started with MCUXpresso SDK for EVK-MIMXRT1020.pdf under the SDK path:
SDK_2.7.0_EVK-MIMXRT1020\docs
Then you can follow it to import the bootloader code to the MCUXpresso IDE:
If you still have questions about it, please kindly let me know.
Wish it helps you!
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Thanks Kerry ,
I have downloaded the latest SDK with all the Middlewear selected , was able to import the project in the IDE , Thanks , that was helpful in need of the time .
Thanks and regards
Naren Chandra
Hi Naren chandra,
You are welcome!
Do you have any other questions about this topic?
If you still have questions about it, please kindly let me know.
If your question is solved, please help me to mark the correct answer, just to close this question, thanks.
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------