How to configure a memory controller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to configure a memory controller

Jump to solution
3,194 Views
rans
Senior Contributor I

Hello,

 

We plan to use the following memory configuration with iMX RT1050 using HyperBUS:

As you can see below there are 4 memory units:

1. HyperRAM memory unit which contains connected with hyperBUs and CS1.

2. HyperFLASH memory unit which contains connected with hyperBUs and CS1. (switch decides if CS1 is connected to Hyperram from section 1 or hyperFlash from section2) 

3. HyperFLASH memory unit which contains connected with hyperBUs and CS2.

4. QSPI flash connected through qspi bus.

 

 

           ---HyperBUS-----------------------------------------------------------------------------------------

                                                                                                                                          | (hyperbus)

            ---CS1-----------------------------------------------------/  (switch)--------HyperRAM ------ |

                                                                                       \------------HyperFlash (boot) -----|

MCU                                                                                                                                  |

            ---CS2-------------------------------------------------------------------------HyperFlash -------- 

 

            ---QSPI------------------------------------------------------------------------QSPI FLASH

 

Does this configuration requires specific settings in memory controller or is it supported out-of-the box in MCUExpresso FreeRTOS ?

If it does - how do we configure the memory controller to support this configuration (Is it described in documentation) ? 

 

Thank you,

ranran

1 Solution
2,842 Views
igorpadykov
NXP Employee
NXP Employee

Hi ranran

there are appnotes on below link like AN12239 How to Enable HyperRAM with i.MX RT,

AN12183 How to Enable Debugging for FLEXSPI NOR Flash which may be helpful

for configuring such setup

i.MX RT1050 MCU/Applications Crossover Processor | Arm® Cortex®-M7 @600 MHz, 512KB SRAM |NXP 

Linux (at91) kernel may not support it, note nxp does not support this kenel so may be useful

also post this on corresponding kernel mail list.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
2,843 Views
igorpadykov
NXP Employee
NXP Employee

Hi ranran

there are appnotes on below link like AN12239 How to Enable HyperRAM with i.MX RT,

AN12183 How to Enable Debugging for FLEXSPI NOR Flash which may be helpful

for configuring such setup

i.MX RT1050 MCU/Applications Crossover Processor | Arm® Cortex®-M7 @600 MHz, 512KB SRAM |NXP 

Linux (at91) kernel may not support it, note nxp does not support this kenel so may be useful

also post this on corresponding kernel mail list.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------