How to access of 0x31000000 address in IMXRT1170

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to access of 0x31000000 address in IMXRT1170

1,672 Views
Nagaveni
Contributor II

Hi ,

I am using IMXRT1170 board.

How can I access the external QSPI flash memory from address 0x31000000? In My application I am getting bus fault when I was trying access the particular address.

My application is working up to 0x30F00000 address.

Please let me know. How to configure ...? 

Thanks In advance.

 

0 Kudos
Reply
8 Replies

1,629 Views
Masmiseim
Senior Contributor I

Hello,

 

Just two questions.

Is the correct size of the flash configured in the Register FLEXSPI_FLSHCR0?

Is the MPU configured correctly for the FlexSPI Memory mapping?

 

Regards

0 Kudos
Reply

1,647 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Nagaveni ,

   Thank you for your interest in the NXP MIMXRT product, I would like to provide service for you.

   What's the flash size you are using? Whether it can support up to 1000000 or not?

  If you are using the MIMXRT1170-EVK board, the onboard flash is the IS25WP128-JBLE.This is the 128Mbit, which size is 0X1000000, it means the accessable range is 0X30000000 to 0X30FFFFFF.

  That's why you can't access 0X31000000, as your flash can't support it.

 

Wish it helps you!

Best Regards,

Kerry

0 Kudos
Reply

1,625 Views
Nagaveni
Contributor II

Hi Kerry,

We have custom board of IMXRT1172 and falsh size is 512Mbits(IS25WP512M-JLLE). please let me know how to configure to access of 0x31000000 addresse

0 Kudos
Reply

1,440 Views
Nagaveni
Contributor II

Hi Keery ,

Thank You for your response,

I have changed the size as you suggested But still I am getting same Bus fault  

Nagaveni_0-1706698907584.png

Please let me know if any changes required,

Thanks In Advance

0 Kudos
Reply

1,430 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Nagaveni ,

  I know why you meet this issues, it is related 3B/4B read commander, as your accessed memory is larger, you need to use the 4Byte address, you can refer to this blog:

https://www.cnblogs.com/henjay724/p/13374775.html

You need to use the 4FRD to replace the FRD.

kerryzhou_0-1706768897545.png

Please try to use 4byte commander to access it again.

If you still have issues about it, please kindly let me know.

Best Regards,

Kerry

 

0 Kudos
Reply

1,361 Views
Nagaveni
Contributor II

Hi Keery, 

Thank you for your response,

I Converted 3B to 4B by modifying cutomLUT of flash as per the data sheet IS25WP512M-JLLE

Modified evkmimxrt1170_flexspi_nor_config.c by replacing 0xEb with 0xEC and 0x18 with 0x20

Nagaveni_2-1707018733241.png

The strcture flexspi_device_config_t deviceconfig In flexspi_nor_polling_transfer.c is modified as below

Nagaveni_3-1707018824828.png

In flexspi_nor_polling_transfer.c , CustomLUT is modified by replacing 0x03 with 0x13

Nagaveni_4-1707019068934.png

replaced 0x0B with 0x0C 

Nagaveni_6-1707019270611.png

Replaced 0xEB with 0xEC

Nagaveni_7-1707019349860.png

replaced 0xD7 with 0x21

Nagaveni_8-1707019510705.png

 

I tried modifing as above , still Unable to access the 0x31000000 address, please let me know if I  missed any steps,

Thanks In advance

 

 

 

0 Kudos
Reply

1,320 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Nagaveni ,

   Thanks for your updated information.

  You mentioned: still Unable to access the 0x31000000 address

How do you access it? Use the code or AHB read the address directly in the IDE?

  What about the erase to the high address range? I mean:

flexspi_nor_flash_erase_sector

  Whether it returns success or not?

  You also can share some screen about your issues, it will help me to check it.

 If you still have issues about it, I also need to apply for one flash which you are using to test it. 

But, it may need more time, as I lack the chip now, and we also will in the Chinese spring Festival Holiday, I may help you to test it after Feb. 19.

Thanks a lot for your understanding.

Best Regards,

Kerry

 

 

0 Kudos
Reply

1,582 Views
kerryzhou
NXP TechSupport
NXP TechSupport

HI @Nagaveni ,

Change the flash size range:

kerryzhou_0-1705655937350.pngkerryzhou_1-1705655943023.png

 

Wish it helps you!

Best Regards,

Kerry

 

 

0 Kudos
Reply