How many MAX_FACES_STORAGE at SLN-VIZN-IOT?
Can add more in SLN-VIZN-IOT?
How can affect at recognition time?
Thanks in Advance
Oscar
Hi Oscar,
How many MAX_FACES_STORAGE at SLN-VIZN-IOT?
The number of faces that can be stored on the SLN-VIZN-IOT is 200 faces.
How can affect at recognition time?
In general, on the SLN-VIZN-IOT the time to recognize a face is more dependent upon the model in use rather than the number of faces stored in the face database. There is a slight dip in recognition performance the more users you add, but in our testing this dip in performance has been negligible enough that we aren't concerned with it.
Have a great day,
Victor
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct"button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Thanks Victor
If I need 1000 or 2,000 faces.
What do you recomend me?
If I put a network with a 5 or 20 devices, how can I sincronize?
Do you have SQL database access? or I can doit?
Thanks in Advance
Oscar
El 26/05/2020 a las 05:02 p. m., victorjimenez escribió:
>
NXP Community
<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
>
Re: How many MAX_FACES_STORAGE at SLN-VIZN-IOT?
reply from Victor Jimenez
<https://community.nxp.com/people/victorjimenez?et=watches.email.thread>
in /i.MX RT/ - View the full discussion
<https://community.nxp.com/message/1317625?commentID=1317625&et=watches.email.thread#comment-1317625>
>
Hi Oscar,
Sorry for the late response, I was checking this with the design team of the solution.
If I need 1000 or 2,000 faces.
What do you recomend me?
Unfortunately for the moment, there aren't any official recommendations on how to deal with this type of request. I apologize for the inconvenience that this might cause you.
If I put a network with a 5 or 20 devices, how can I sincronize?
Do you have SQL database access? or I can doit?
We don't have any official support for this either. You will have to implement this on your own.
Regards,
Victor