How does core clock affect uboot/kernel?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How does core clock affect uboot/kernel?

1,612 次查看
alain_olivier
Contributor I

Hello,

I plan to use IMXRT1021 for a project, but I notice the industrial and customer versions have a different core clock, 400 MHz and 500 MHz respectively. Is switching from one to the other something transparent or does it require uboot/kernel adjustments?

Thanks,

Alain.

标签 (1)
标记 (3)
0 项奖励
回复
1 回复

1,544 次查看
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Alain Olivier

The difference between the Industrial and the Consumer is the temperature range, level of accuracy with the voltage, freq, etc. So this is why the Frequency change between that datasheet. Since the image for uboot is chip specific, there should not change anything on this, but the uboot image should consider what chip would use.

Regards

Jorge Alcala

0 项奖励
回复