Hang up while enabling/disabling break point during debug session

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Hang up while enabling/disabling break point during debug session

1,916 次查看
JayeshPatel
Contributor I

After launching debug session, tool just hang up while actively enabling/disabling break point. Seems it trying to update FLASH when activates the break point which causes hang up.

0 项奖励
回复
4 回复数

1,847 次查看
JayeshPatel
Contributor I

Processor MIMXRT1176xxxA_M7

0 项奖励
回复

1,853 次查看
JayeshPatel
Contributor I

Following are the processor/setup.

Tool: MCUXpresso IDE v11.7.1 [Build 9221] [2023-03-28]
Processor: I.MX RT 1170
Debugger: J-Link Plus Compact (Segger)

Yes, I am still experiencing the issues.

Steps:

1. Download code through debugger. Code is running fine

2. Click Suspend (Halt) on the tool

3. Put bunch of break points in different files

4. Click Resume on the tool

5. Sometime it runs and hit the breakpoint. (Some times it just hangs up)

6. If above step is successful, it will half on the break points. Some time if hangs up if remove break-point and click Resume.

7. If above steps are successful, it will eventually hangs up after hitting breakpoint few times.

Only thing can be at this point is, Terminal debug session and start new session.

0 项奖励
回复

1,805 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @JayeshPatel,

Thanks for clarifying. Please try updating your IDE to the latest version (v.11.10.0) and let me know if you still experience the same issues. It can be downloaded from the following website: MCUXpresso IDE for NXP MCUs | Linux, Windows and MacOS | NXP Semiconductors | NXP Semiconductors

BR,
Edwin.

0 项奖励
回复

1,857 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @JayeshPatel,

Are you still experiencing this issue? How are you enabling/disabling the breakpoints? How do you start the debug session? What IDE and SDK versions are you using? What i.MX RT part?

BR,
Edwin.

0 项奖励
回复