From which memory IMXRT1020 EVK example codes are executed ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

From which memory IMXRT1020 EVK example codes are executed ?

1,640件の閲覧回数
narenchandra401
Contributor III

Hi all ,

Since IMXRT 1020 is a cross over processor , which is basically a MCU with a extenal memory , How do i know into which external memory is IMXRT1020 EVK Example codes are flashed into and are executed from , in the example code where do i find the settings or is it done with the IDE settings ?

Anticipating a quick response 

Thanks and regards 

Naren

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,568件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi Naren,

 

SDK examples boot from IS25LP064 64 Mb QSPI Flash. The Flash driver is selected in the properties of the project.

pastedImage_1.png

The settings of this memories are located in the located in the flexspi_nor_confg file in the xip folder.

 

Best regards,

Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信