FlexSPI control NORFLASH

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FlexSPI control NORFLASH

1,835 Views
zhangyanming
Contributor I

Lately, i use i.MX RT 1052 to do a project.In the project,i want to use the FlexSPI to control two same NORFLASH,one is controllede by portA ,i wang to use this to storage code,the code is implemented in XIP mode.the other one is controlled by portB,i want to use this to storage data.Now,the question is one FlexSPI can realize this function?If it is feasible,how to realize?If it is not feasible,why?

thanks.

0 Kudos
Reply
1 Reply

1,719 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please refer to the following:

FlexSPI control NORFLASH 

https://community.nxp.com/message/1070474 

Regards,

Yuri.

0 Kudos
Reply