FlexIO3 module external trigger

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FlexIO3 module external trigger

1,350件の閲覧回数
mail10
Contributor II

Hi,

In the imxRT1060 manual (IMXRT1060RM.pdf) isn't any description the FlexIO3 module external trigger source (selected by TIMCTLa.TRGsrc=0). Who can the FlexIO3 be external triggered?

 

Best regards,

Reiner

0 件の賞賛
返信
1 返信

1,342件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello,

I checked the RM, there is not the limit for the FlexIO3 module external trigger source.
Please note:FLEXIO1 and FLEXIO2/3 parameters are not exactly the same. Hope it help you. Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 件の賞賛
返信