Flex CAN Self Test / Loop back mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flex CAN Self Test / Loop back mode

2,233件の閲覧回数
basu_gouda
Contributor I

Hi,

I am trying to implement the self test mechanism for Flex CAN on RT1176 , for which I am using the internal loopback mode for implementing the self test of the Flex CAN module. However I would love to know if any failure causes can be detected for the same as the reference module does not give much of the details on the same.

I meant that if the Loop back fails to receive the message it transmitted, any mechanism on detecting the same.

 

Thanks in Advance

Basavanagouda

タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,193件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
I hope you are well.

Yes, in loopback mode errors can be detected.

Best regards,
Omar

0 件の賞賛
返信

2,162件の閲覧回数
basu_gouda
Contributor I

Hi Omar,

 

Thanks for your response,

Can you please elaborate on the same, will it be associated with the rx error mode signal or need to monitor any other source.

The reference manual does not give the clear answer.

 

Thanks in advance

Basavanagouda Ganganagoudar

0 件の賞賛
返信

2,145件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

The error detection is related to the methods described in 66.3.14 from the RM.

Best regards,
Omar

0 件の賞賛
返信