Flex CAN Self Test / Loop back mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flex CAN Self Test / Loop back mode

2,235 Views
basu_gouda
Contributor I

Hi,

I am trying to implement the self test mechanism for Flex CAN on RT1176 , for which I am using the internal loopback mode for implementing the self test of the Flex CAN module. However I would love to know if any failure causes can be detected for the same as the reference module does not give much of the details on the same.

I meant that if the Loop back fails to receive the message it transmitted, any mechanism on detecting the same.

 

Thanks in Advance

Basavanagouda

Tags (1)
0 Kudos
Reply
3 Replies

2,195 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
I hope you are well.

Yes, in loopback mode errors can be detected.

Best regards,
Omar

0 Kudos
Reply

2,164 Views
basu_gouda
Contributor I

Hi Omar,

 

Thanks for your response,

Can you please elaborate on the same, will it be associated with the rx error mode signal or need to monitor any other source.

The reference manual does not give the clear answer.

 

Thanks in advance

Basavanagouda Ganganagoudar

0 Kudos
Reply

2,147 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

The error detection is related to the methods described in 66.3.14 from the RM.

Best regards,
Omar

0 Kudos
Reply