Flex CAN Self Test / Loop back mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Flex CAN Self Test / Loop back mode

2,247 次查看
basu_gouda
Contributor I

Hi,

I am trying to implement the self test mechanism for Flex CAN on RT1176 , for which I am using the internal loopback mode for implementing the self test of the Flex CAN module. However I would love to know if any failure causes can be detected for the same as the reference module does not give much of the details on the same.

I meant that if the Loop back fails to receive the message it transmitted, any mechanism on detecting the same.

 

Thanks in Advance

Basavanagouda

标记 (1)
0 项奖励
回复
3 回复数

2,207 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
I hope you are well.

Yes, in loopback mode errors can be detected.

Best regards,
Omar

0 项奖励
回复

2,176 次查看
basu_gouda
Contributor I

Hi Omar,

 

Thanks for your response,

Can you please elaborate on the same, will it be associated with the rx error mode signal or need to monitor any other source.

The reference manual does not give the clear answer.

 

Thanks in advance

Basavanagouda Ganganagoudar

0 项奖励
回复

2,159 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

The error detection is related to the methods described in 66.3.14 from the RM.

Best regards,
Omar

0 项奖励
回复