Hi sir,
1)Is it possible to remap the internal flash(4MB) address using flash remapping method in imxrt1064?
2) Is it XIP mode is supported in internal flash on imxrt1064?
thanks and regards
Karthik N E
Solved! Go to Solution.
Hello Karthik N E,
1)Is it possible to remap the internal flash(4MB) address using flash remapping method in imxrt1064?
Yes, it is possible to remap the on-chip flash
2) Is it XIP mode is supported in internal flash on imxrt1064?
Yes, XIP is supported in the on-chip flash of the RT1064
Have a great day,
Victor
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hello Karthik N E,
1)Is it possible to remap the internal flash(4MB) address using flash remapping method in imxrt1064?
Yes, it is possible to remap the on-chip flash
2) Is it XIP mode is supported in internal flash on imxrt1064?
Yes, XIP is supported in the on-chip flash of the RT1064
Have a great day,
Victor
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------